-
- Inspection machine
- Transparent object inspection
Transparent Object
Inspection SystemIS-UVCL01You won’t miss it,
even if it’s not visible!Transparent materials such as glass and synthetic resin are essential for our daily lives. CKD supports the quality and safety of these products. CKD’s proprietary solution solves the cost and risk of visual inspections of transparent objects. 
1. Significantly reduces inspection leakage risk during visual inspection of transparent objects
Until now, in the manufacturing process of transparent materials such as glass and film, the detection of product defects has been dependent on visual inspection. CKD will develop the IS-UVCL01, the first transparent object inspection system in the inspection industry, to improve the quality of many manufacturing processes and to work on labor reduction and unmanned operation.
2.Easy installation by considering “setting to existing environments” and “space saving”
This device has a compact design and can be mounted on various production lines. The minimum configuration of camera, lighting, and processing equipment is provided for easy customization to suit the customer’s manufacturing processes.

Perforated [Cup container]
Detects holes in the bottom of transparent cups Inspection target example [Cup container]
- Food container [Box lunch] [Tofu] [Jelly]
- Cosmetic container
- Research and industrial plastic containers
Split [glass bottle]
Detects the refraction of the crack light on transparent glassInspection target example [Glass product]
- Glass plate
- Syringe
- Vial Bottle
Different thickness [jelly container]
patent pending
Detects differences in the thickness of containers from the amount of transmitted lightInspection target example [Film product]
- PVC
- PP
- PE
- PET
Liquid leakage [inside soft capsule]
Detects the difference in fluid permeability in capsulesInspection target example [Liquid]
- drug