Brand Slogan![]()
On April 2, 2023, the CKD Group established the brand slogan "Creating Solutions Together" which strongly expresses our thoughts and actions for the future. This slogan expresses our desire to work together with our customers, business partners, and CKD employees to explore and co-create automation technologies with creativity and innovation, to solve environmental and social issues, and to create a prosperous future.


MOVIE
Here are some of our activities around the world.
HISTORY
We would like to introduce the history of development of our two core businesses, "Automatic Machinery" and "Component Products" in the 80 years since our establishment.



The company was founded in what is now Meieki Minami 2-chome, Nakamura-ku, Nagoya City. Five prominent companies invested in the Company and started manufacturing and selling electrical parts for airplanes.



With a shortage of workers and all kinds of goods, it was not easy to start production.

Our business objective was to "manufacture, repair, and sale of electrical machinery and apparatus". After the war, we made everything that was needed.



The "Vacuum Tube Manufacturing Machines" and the "Tube Manufacturing Machines" were developed to automatically manufacture glass tubes that contain electrodes, which were indispensable for vacuum tube manufacturing.


After repeated trial and error regarding the technically difficult configuration of the machine, the Company succeeded in developing an automatic dry cell battery manufacturing line. The Company gained a reputation for automation technology and plant development.


Utilizing the technology related to the heat treatment of glass, the company developed an "automatic filling machine for glass injection ampoules". This led to the later business of pharmaceutical packaging machinery.

It is applied to the vacuum filling process such as filling machines for lotions and sake (Japanese rice wine) bottling. It was also developed for Western spirits and synthetic spirits, and secured the entry into the brewing industry.




Introduced the world's highest standard of flourescent tube and semiconductor manufacturing technology.
With the spread of TVs and automobiles, demand for tube manufacturing equipment to produce miniature vacuum tubes and shielded beams grew rapidly.

CKD had been manufacturing solenoids in-house for the tube manufacturing machinery for some time and developed the "A Series", the original AC solenoid, based on those solenoids.


Considering that solenoid valves should be used for various automatic controls, we developed solenoid valves with a packing-free structure that is not limited to conventional solenoids.


Along with the "Automatic Machinery Manufacturing Department", the "Components Manufacturing Department" was formally established.

In order to pursue efficiency and ease of use, the machinery and assembly plants were separated, and the layout within the machinery plant was clearly divided into machining and precision machining.


A machine capable of packaging 600 pieces of chewing gum per minute. The reputation of the new wrapping machine spread throughout the confectionery industry, resulting in explosive sales and market penetration.

A table-top turret drilling machine with a capacity equivalent to six single-axis drilling machines, with six drills up to 6 mm in diameter, was developed.

Commercialized Japan's first cylinder with a solenoid valve, the "Cell Cylinder CAV Series".


The fully-automatic "Automatic powder weighing and wrapping machine" was easy to operate, trouble-free, and could freely use polyethylene, cellophane, and other packaging materials.


Exhibited the High Speed Strip Packaging Machine, a high-speed automatic packaging machine for tablets, and the JC Cartoning Machine, a box-packing machine for chocolates, at the largest packaging exhibition in the U.S.
Equipped with a six-bag packaging function, this machine was developed to continuously package instant noodles, sandwiches, candies, cookies, and other solid products with heat-sealable film.

This is an automatic indexing table using pneumatic pressure. The RTA-420 employed a cylinder with valve for the driving force and a hydro-check cylinder for stable feed speeds.


It was a compact tabletop machine for small-diameter hole machining. In the era when there was no machining center yet, it had an innovative function to be able to change tools instantaneously while still being manually operated.


We developed the D-blister packaging machine, a vacuum forming and packaging machine for pills. The transparent film allows products to be displayed as they are, and the machine is hygienic, revolutionizing the pharmaceutical packaging format.


This new stand-alone machine was developed for the chewing gum packaging machine's pre- and post-processes: gum arranging, gum breaking, gum cutting, and forming caser machines.

In response to customer demands, we researched and developed various products (products produced from machines), including compass assembly machines and baby bottle nipple hole drilling machines.


We began our own research on the "caulking method", which is the key to electrolytic capacitor assembly machines, and created excellent assembly machines by utilizing the technology we had cultivated.


As a new solenoid valve with a completely different actuator structure from conventional ones, we developed the "Capsule Mold Solenoid Valve MU type".




The fully automatic tray packing machine, automatic weighing machine, and printer for packing meat and fresh food on styrofoam trays were developed.

Through technological innovations in pinboard control and pneumatic circuits, CKD has created products for the pneumatic industrial robot "SERUAMU".


CKD had previously exported "lighting-tube machines" via a trading company, but directly negotiated to export a "decorative lighting bulb machine" to GE Corporation in the U.S. It was the first exported machine by CKD.

In response to the demand for automated water sprinkling, we developed the RSV type solenoid valve "Rainbow System". The system was used in the agricultural field and as a watering system for golf courses and other greenery applications.


We developed the "CHIROMATTO", an automatic deep-drawing vacuum packaging machine.Suitable for packaging hams, sausages, fish cakes, frozen foods, etc.

The corporate logos, colors, slogans, and product slogans, and other systems were unified to renew and revitalize the corporate image.


We developed a capacitor element winding machine that can be manufactured by inputting data, and a "VALSER Series" for the electronic component industry.

The "Selex Valve 4F Series" was developed to meet the needs for low wattage and oilless solenoid valves to stabilize quality and save energy.


Foods often lose their flavor when heat-sterilized after packaging. The Aseptic Pack MM machine fills and packs food under aseptic conditions and enables long-term preservation.

Small direct-acting solenoid valves were developed, bringing the number of models from several dozen to several hundred thousand through the combination of parts.


With the gradual computerization of the industrial and consumer electronics industries, and the resulting customization of control systems and kits, the automation of this production became an urgent task.


The company's attitude toward a major rebirth was demonstrated both internally and externally to enhance its image.
Consisting of a monitoring camera and a sheet ejection mechanism, it reliably sorts and eliminates pills regardless of their shape if 7% or more are chipped.
Developed the "PV5 Series" of ISO valves.


We developed a flexible packaging system for small-box corrugated cardboard casers, which is drawing attention from the packaging industry as a technological innovation system.


This product was well received for use in small-scale pneumatic systems because it could be programmed directly along with machine movements by those who could not set up relay sequence circuits.




The "AMB Series" of air-operated valves for chemical solutions was developed in response to requests for the development of air-operated valves for chemical solutions, as solenoid valves for chemical solutions were not compatible.


54 products of pneumatic components and control components were selected in the newly established Industrial Machinery category, and the "Pneumatic valve" was awarded the Grand Prize (currently the Gold Prize) in the category.


With a policy of full-scale entry into the semiconductor manufacturing equipment market, the company launched the concept of "Fine Components" with respect to its product line.

While there was a growing trend toward labor saving, orders for large-scale machinery increased partly due to the demand for production lines of machinery. It has also expanded into new industries such as video vending machines and food packaging machines.

Parallel cam with parallel input and output shafts.The development of this product was based on aggregated needs.


The modular design of the "SELEX FRL 4000 Series" that allows compact interconnection, won the Design Awards in Japan and Germany.



The CFF-360 is a high-capacity, multi-functional food wrapping machine with easy mold attachment and removal, easy positioning of each device, and the ability to freely add units for refilling, vacuum packaging, gas displacement packaging, and other functions.


High precision, space saving, miniaturization, and lighter weight were expected by the unitization of elemental components used for automatic assembling equipment, and unit cylinders were developed accordingly.


With the increasing number of women entering the maintenance and servicing field and the consequent demand for ease of operation and simple operation, we developed the "Blister Pack U" Series, which can change molds with a single bolt.

The ABSODEX "AX Series" was developed with the aim of high precision and flexible indexing units.


The solenoid valve "4T Series" has a unique shape with solenoids concentrated on one side, enabling easy wiring and piping and allowing flexible reconfiguration of manifolds.


CKD's first laser-based 3D image processing technology was commercialized.

Production of 8,000 lamps per hour was realized on the FL high speed line.

The "EV Series" pressure proportional control valves improved quality and productivity by introducing proportional control valves, and we expect to see a significant increase in demand with the progress of factory automation.


We launched the "HYW Series", a large-size series of water-cooling equipment that incorporates the needs of the times, and the "Xeroaqua (zero aqua)", which completely changed the concept of dryers.


Based on the concept of kindness and strength such as affinity, trust, tone and humanity, the logo has been changed from a straight line to a softer logo.





It supports factory automation by performing "gripping, moving, rotating", and other operations at high speed and with precision even in environments where there is no air.


With the spread of flat-screen TVs and plasma TVs, CKD developed a machine to manufacture backlights that illuminate thin LCDs from the rear.


We developed an inspection system that simultaneously solves the three problems of "pharmaceutical safety", "environmental friendliness", and "automation of visual inspection".

The "MN3E0 and MN4E0 Series" of small solenoid valves contribute to thin and space-saving design, significantly reducing installation space.


The FBP-600E blister packaging machine was developed based on the concept of "environmental friendliness", further refining the high quality and ease of use that have been cultivated to date.


The "SCG and STG Series" respond to the needs for environmental protection and pollution prevention as typified by RoHS and other regulations.


The Medical Blister "MBP-500M", a machine that is effective for small lots of multiple products, was released.


The "P4 Series", which supports the latest rechargeable battery production process, has been launched by aggregating models with proven track records in automatic machinery.


The pneumatic cylinder "SSD/LCR type" electric actuator was developed for "end control, multi-point positioning, pitch feed", etc.


The "SMG Series" space-saving cylinders used in assembly and inspection equipment for precision components and IC devices was released.


A pharmaceutical packaging machine was developed to meet the requirements of suppression of scattering of chemical dust, protection of workers, and prevention of contamination to other products.

Released the industry's smallest class Desktop DD actuator "ABSODEX AX6000M Series".




Based on the concepts of safety, environment, ease, and design, the CFF-360E has been enhanced with environmental considerations and safety features such as reduction of waste materials and air consumption.

As a human-friendly product, it contributes to creating a safe and comfortable working environment for seniors and women.


Pillow packaging machine, a post-process of blister packaging machine, was launched to align the entire packaging line.

The pilot operated 3, 5-port valve "4G*R Series" has achieved 100 million endurance cycles with a special surface treatment.

A lineup of safe and reliable equipment for food production has been developed and branded.


The "PEW-380" was able to manufacture square lithium-ion batteries used in electric vehicles and PHVs at high speed, with high precision.


The new pharmaceutical pill packaging machine "FBP-320E" that pursued ease of use and safety, received the Machinery Industrial Design Award the following year.

The "NS Series" was developed to easily supply nitrogen gas for antioxidation and explosion-proof applications.


In-line tablet inspector "Flash Patri FP-U Series" was released, which can inspect misalignment of cutting position and sheet printing after pills are packaged.
The lineup includes the compact and highly rigid EBS, the EKS which achieved the industry's highest speed and acceleration/deceleration, and the EBR rod with a built-in guide.


Received the Kids Design Award and the Good Design Award in recognition of the company's efforts.


Three-step multi-resolution switching function enables inspection of a wide range of fine inspection targets. Equipped with an easy-to-view and easy-to-use touch monitor.

Longer service life reduces the number of replacements and the time loss when equipment stops operating, and also reduces the amount of waste by reducing the frequency of discarding malfunctioning products.


The nitrogen gas extraction unit "NS Series" and the high durability component "HP Series" were highly evaluated as contributing greatly to the reduction of the environmental load and the achievement of SDGs.


In order to realize high quality, stable production, and low cost, a new packaging machine with Japanese quality produced in China was introduced to the Chinese medical market.

Facilea, a visual programming tool, was launched as an easy-to-use application for automating inspection processes that required specialized knowledge.


Utilizing the CKD's strength in inspection technology cultivated in the pharmaceutical market, we launched the "IS-UVCL01", a device that automatically inspects for defects in transparent materials, which are mainly done through visual inspections.

The RLSH, RHLF, and RCKL Series pneumatic grippers for cooperative robots from Universal Robotics were developed.


Under the concept of high reliability, ease of selection and ease of use, we released the "Multi-fit valve" which is an eco-friendly multi-fluid control with long service life and power savings.


To commemorate our 80th anniversary, we established our "Purpose" and "Brand Slogan" in April, and our "Values" in October 2023.


Three companies from different industries collaborated to successfully commercialize PTP packaging using environmentally friendly biomass plastic. They received the "Minister of the Environment Award" at the 5th Japan Open Innovation Awards.
Achieving durability of over 120 million cycles (under CKD testing conditions), this plug-in valve pursues high durability. It is also designed to minimize air leakage even during long-term use or when equipment is idle, contributing to the reduction of CO₂ emissions.


Based on the concept of co-creation with customers, this showroom allows visitors to experience the appeal of products in an impressive space filled with various content. "ulu" means "to grow" in Hawaiian, and the aim is to grow together with visitors and create new innovations.


We held our first-ever technology exhibition, created through the collaborative efforts of production, sales, and staff. Engineers themselves promoted the diverse technologies that we have explored and co-created with our customers, business partners, and colleagues.


Through its proprietary sheet transport and scrap recovery technologies, the company not only reduced plastic usage by more than 7% compared to conventional methods, but also reduced plastic waste generated during the PTP sheet manufacturing process by more than 70%. The product was branded as ClearE-Sheet, and branding activities were conducted accordingly. The company received the World Star Award, the Asia Star Award, and the Japan Packaging Award.

In "blow-out operations" that consume large amounts of compressed air in production sites, this technology reduces air consumption by up to 75% and electricity consumption by intermittently controlling the blow-out process at arbitrary intervals. It received the Director-General's Award from the Agency for Natural Resources and Energy (Electricity Demand Optimization Field) in the Product/Business Model category of the 2025 Energy Conservation Awards.


At the "Future Society Showcase Project," specifically the "Future Life Expo/Future Life Experience," we exhibited a new type of TV game where characters are controlled using a controller that utilizes air pressure and digital technology.


We have developed a new stacking machine, the "HCA-220S," which meets the diverse packaging needs for pharmaceutical PTP sheets while achieving a space-saving design and high productivity.

In addition to Facilea's functionality and ease of use, it features more advanced image processing capabilities. It supports the GenICam standard, significantly increasing the number of compatible devices. It also flexibly handles template matching for workpieces of different sizes and with 3D tilts.

© 2023 CKD Corporation.