FAQ

We’re Here to Answer Your Questions.

  1. Component Products TOP
  2. The Compact Arm
  3. FAQ

Click to View Answers

  • Q

    What is the maximum weight capacity of the Compact Arm?

    A

    Size L supports up to 5kg, and Size H supports up to 15kg. (including the weight of the jig that supports tools, etc.)

  • Q

    What types of tools can be used with the Compact Arm?

    A

    The Compact Arm has a proven track record with tools such as impact wrenches and nut runners. The Compact Arm has a proven track record with tools such as impact wrenches and nut runners.
    It can also be used with a variety of other tools.

  • Q

    How are tools mounted to the Compact Arm?

    A

    Tools can be mounted using various methods, including bottom mounting, ball joints, flanges, and clamps.
    Please refer to the mounting images for more information.

  • Q

    What is the approximate cost of the Compact Arm?

    A

    The list price starts at ¥419,360 JPY.

  • Q

    How is the Compact Arm installed?

    A

    The Compact Arm can be mounted on an aluminum frame, etc. with a mounting width of 60 mm.

  • Q

    Are there any specific environmental requirements or preparations for installation?

    A

    Customers will need to provide their own air source.

  • Q

    Are tours or demonstrations available?

    A

    Yes, tours and demonstrations can be arranged.
    Please contact us for more information.

  • Q

    What is the typical lead time?

    A

    The standard lead time is approximately two weeks.
    Please note that lead times may vary depending on specifications and the time of year. Contact us for a precise estimate.

  • Q

    What is the maximum operating pressure?

    A

    For size L, it is 0.25 MPa, and for size H, it is 0.45 MPa.

  • Q

    Are there any consumable parts?

    A

    The packing kit and shock absorber are considered consumable parts. (Contact CKD when other parts are required.)