Press fit
/ EBR・GSSD2
Requests and Issues
The rod type actuator requires provision of a guide side by side, and the number of components is increased.
Since various kinds of workpieces are being conveyed, an electric actuator is desired, but it should be installed in a space saving way as possible because of the limited space.
Recommendations
The EBR-M and EBR-G Series and GSSD2 Series are recommended.
EBR-M・EBR-G Series
GSSD2 Series
The Rod type EBR-M/EBR-G Series have a guide built into the body, eliminating the need to install guides for certain loads. Therefore, it can be used with minimal foot space, contributing to space saving of the entire equipment.
In addition, since there are no mechanical parts required when a guide is installed, this contributes to not only space saving of equipment but also reduction of design and assembly work-hours.
The guide rails contain balls to reduce friction and ensure smooth movement.
For maintenance, mounting holes can be directly installed on the top and bottom of the body without disassembling the product, enabling rapid operation in confined spaces.
View EBR-M/G
product information
View GSSD2
product information
The GSSD2 Series has the same rigidity as the SSD2 Series, since the body is common to the pneumatic components Compact Cylinder SSD2 Series.
Normally, when replacing pneumatic components with electric motion components, the size of the electric device may seem larger if the same rigidity is to be achieved, but the GSSD2 Series can replace the SSD2 Series with the same size and rigidity.
Since it is connected to the ECG Series controller and the ECMG Series multi-axis controller, which are common to other types of actuators, the controllers can also be standardized, contributing to reductions in inventory and man-hours required for management.
You can choose from a total of five interfaces: PIO, IO-Link, CC-Link, EtherCAT, and EtherNet/IP.
※For ECMG, select from CC-Link, EtherCAT and EtherNet/IP.